Cancel
Showing results for 
Search instead for 
Did you mean: 

Filling large area with holes

Experimenter
Experimenter

I am drawing a screen and need to place a large amount of spaced holes. Which is the quickest way of doing this, as i am new to cad drawing

 

Thanks

 

Stewart 

5 REPLIES

Re: Filling large area with holes

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I'm assuming you are doing this in Solid Edge Draft since this is the 2D forum.

 

Draw the elements you want to pattern at the start point of where you want the pattern  Then on the Sketching tab in the Draw area, you can find the Rectangular and Circular Pattern commands.  Follow the prompts.

 

I would also suggest trying command finder at the bottomof your screen to help you find commands like this.

 

2016-08-10_8-59-12.png



Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com

Re: Filling large area with holes

Experimenter
Experimenter

Thank you for your help

 

Stewart

 

Re: Filling large area with holes

Experimenter
Experimenter

Hi

 

I have gone to the rectangular command bar, this is not in bold so can not open it up. Is there a reason for this

 

Thanks

 

Stewart

Re: Filling large area with holes

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi Stewart:

  

Can you post a picture of your Solid Edge screen to show what you see is not in bold ?

  

~Tushar

Re: Filling large area with holes

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @Stewartc67,

 

Here is a short video of a rectangular pattern....hopefully the steps are clear.

You may notice, at the end, I right click on the pattern and select "ungroup", this is because by default, Solid Edge will automatically "group" the resulting pattern. [only necessary, if wanting to crop instances off, like I showed]

 

(view in My Videos)

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x3 seats]
Windows 10 - Quadro P2000
Testing: Solid Edge 2019