Cancel
Showing results for 
Search instead for 
Did you mean: 

First impression Solid Edge 2019

Legend
Legend

What are your first impressions of the wonderful new release;

 

Positive;

- Snappier, quicker

- Quicker update of drawings

- Easier to get views up-to-date if model is out of date.

 

Negative;

 

Please share

 

 

Jan Bos

Emmen, The Netherlands

User since Solid Edge V3.5

 

 

 

 

11 REPLIES 11

Re: First impression Solid Edge 2019

Genius
Genius

Hi Jan,

 

I received an email from our reseller yesterday. They recommend waiting for MP1 since MP0 is an 'incomplete first version' (their words). Can you comment on that? Incomplete in what way?

Re: First impression Solid Edge 2019

Legend
Legend

I have beta tested this version for a few months now.. and as far as I know it is wunderful...  as stated its snappier.. 

 

No problems so far.. 

 

I assume that we have the same reseller, I did not get this warning.. 

 

It is a strange sort of marketing... siemens releases something and than resellers tell customers that they should wait because there is a so called "problem"... 

 

Do a dual install and give it a try it wil not disappoint you.

 

Kind regards,

 

 

Jan Bos

 

 

 

Re: First impression Solid Edge 2019

Experimenter
Experimenter
Didn't see any issues for now, works smooth and quick

Re: First impression Solid Edge 2019

Gears Genius Gears Genius
Gears Genius

Works smooth and quick. I also like the drawing updates and the new Teamcenter interface additions.

 

Cheers

 

Ionman

Re: First impression Solid Edge 2019

Phenom
Phenom

pro's: don't know yet

con's:

bey bey ribon tabs:

CoTfGqNbig file tabs

...........................................................................................................
Solid Edge 2019 & AutoCAD 2020 user

Re: First impression Solid Edge 2019

Phenom
Phenom

uninstall an install fixed the problem.

Strange...

...........................................................................................................
Solid Edge 2019 & AutoCAD 2020 user

Re: First impression Solid Edge 2019

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I noticed my tabs missing as well but just restarting SE was enough to fix that.

I blamed it on my Surface Book at first but someone else reported it also.

LMGi
www.TLMGi.com

Re: First impression Solid Edge 2019

Phenom
Phenom

Strange...

Do you have the read-only problem as well?

open a part from within an assembly makes it read-only.

...........................................................................................................
Solid Edge 2019 & AutoCAD 2020 user

Re: First impression Solid Edge 2019

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Joris

 

 

 

I believe this is the same issue as mentioned in another post.

That behaviour has come from old %appdata% entries from previous versions.

 

Delete them or rename the unigraphics folders there, start SE again and everything was just fine.

 

 

No need for uninstall/install SE

 

 

regards
Wolfgang