Cancel
Showing results for 
Search instead for 
Did you mean: 

Fit vs. Fit

Phenom
Phenom

When we use the "Fit" button onscreen in draft the result is:

Extend_Button.png

This is the desired result.

 

When I click on the button "Fit" on my SpacePilot Pro the result is:

Extend_Fit_3dConnexion.png

Any idea how I can tell the 3D mouse the result has to be the same as the onscreen button?

...........................................................................................................
Solid Edge 2019 & AutoCAD 2020 user
9 REPLIES 9

Re: Fit vs. Fit

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Solid Edge provides two fit mode:

  • Double click with MMB and this will be fit by sheet
  • Shift + Fit command and this will be fit by drawing views. 3D mouse "fit" supports this mode, but you can change this in Solid Edge. Open a drawing and go to Add-in tab and select customzie button in 3D control group...

 

Best,  

Imics
http://solidedgest.wordpress.com/

Re: Fit vs. Fit

Phenom
Phenom

Thanks for your answer!

 

I use ST8 & the mouse driver is version 10.2, I don't have a tab "add-in".

In the customize window I only find the standard "Fit", no "fit by sheet"

 

But:

Thanks to your explanation I managed to make a "macro" and assign this to the buttong, so problem solved. ;-)

...........................................................................................................
Solid Edge 2019 & AutoCAD 2020 user

Re: Fit vs. Fit

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

My (our) friend @Tushar has a great macro here:

link

 

Best,

Imics
http://solidedgest.wordpress.com/

Re: Fit vs. Fit

Phenom
Phenom

The need of knowing code is obsolete for this kind of simple things:

macro.png

...........................................................................................................
Solid Edge 2019 & AutoCAD 2020 user
Highlighted

Re: Fit vs. Fit

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Joris,

 

What is this macro tool you showed above?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Fit vs. Fit

Phenom
Phenom

That's the build-in tool from 3Dconnexion:

macro2.png

...........................................................................................................
Solid Edge 2019 & AutoCAD 2020 user

Re: Fit vs. Fit

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hmmm. Do these macros work without the space devices? For example on keyboard and ribbon?

 

I never got into using the 3D devices and actually prefer the plain vanilla kbd and mouse.

Sort of like smoking or golf, the first experiences were unpleasant enough that I didn't pursue them further and learn to like them or become addicted.

Smiley Happy

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Fit vs. Fit

Phenom
Phenom

I smoked (a lot) but never played golf. 

 

I can't work in SE without a 3D mouse, the time you win, unexpected!

...........................................................................................................
Solid Edge 2019 & AutoCAD 2020 user

Re: Fit vs. Fit

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Joris,

 

I guess I never used it long enough to get the "runner's high". It's better for me to stay plain vanilla anyway in my current role. I help users so I need to be untethered to custom interface hardware. It's bad enough when some users have selected vertical as opposed to horizontal menus.

BTW, would these macros work without the 3D device? Like keyboard shortcuts or ribbon menu?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200