Cancel
Showing results for 
Search instead for 
Did you mean: 

Flashfit & edge

Valued Contributor
Valued Contributor

For positioning a part in an assembly. When you use the flashfit, and hover over a circle, you can select the "Edge", when using that edge to position the part, you automatically get an axial align, but the rotation is locked. Can it be set that it is unlocked by default?

 

thx, Johan

4 REPLIES

Re: Flashfit & edge

Gears Phenom Gears Phenom
Gears Phenom
Hi,

You can't set it up. You have to ask an ER for this! Here is "my" ER7320049!

BR,
Imics
http://solidedgest.wordpress.com/

Re: Flashfit & edge

Phenom
Phenom
Hopefully they not change that behaviour, I do use it to assemble fasteners with 2 click only.

Re: Flashfit & edge

Gears Phenom Gears Phenom
Gears Phenom
Hi,

It will be a win to win business, if Solid Edge remembers last used option (locked or unlocked). I think this should be the best solution for both world! 😁

BR,
Imics
http://solidedgest.wordpress.com/

Re: Flashfit & edge

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

This is one of those many commands, well thought out and implemented, works perfectly for 'most' users, but which needs a setting under its options which a user can 'tweak' to modify a small part of the workflow to suit his unique requirement.