Cancel
Showing results for 
Search instead for 
Did you mean: 

Flat Pattern in one step

Creator
Creator

Hi.

I have question. there is a way how to make more Flat Pattern in one step? Example - I hava 10 sheet metal parts in folder and i need DXF files from Flat Patern. I found Batch Processing Sample to create step files or others but to create DXF files doesnt work. there is somthing like macro for this operation. I dont want cklick 1000times save as flat pattern....


11 REPLIES 11

Re: Flat Pattern in one step

Honored Contributor
Honored Contributor

This is one portion of what "Nesting software" does. I don't use DXF frequently enough to know th best answers. We still print hardcopy and program the punch or plasma manually.

Re: Flat Pattern in one step

Solution Partner Genius Solution Partner Genius
Solution Partner Genius
It is not possible in SE so we have written a program for it
http://www.enginia.nl/solid-edge/40-solid-edge-tools/134-flatten-em
https://www.youtube.com/watch?v=dmsBS3Wyrxo
You can flatten directories or assemblies with it and sort it on a property e.g. Thickness

Re: Flat Pattern in one step

Phenom
Phenom

If you were running a PDM/PLM system I believe that you can build in the steps to export a dxf when a part/document is "released".

Re: Flat Pattern in one step

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@RyanM, I know that Teamcenter will do that, at least can do that, at every save regardless of status.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Flat Pattern in one step

Phenom
Phenom

@bshand Yes that is true. But you would only want to create the data at certain steps along your development workflow. And then make it only visible/accessible to certain people.

 

I wouldn't want this to occur at ever check-in / check out (CI/CO) point.

 

Only when the author feels the file is ready to be built/manufactured. I worked at acompany that had two workflows; 1) for the development cycle and 2) for production which required formal change process. Development cycle used alpha versions and released used numeric revisions.

Re: Flat Pattern in one step

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Actually I'm not sure about dxf. Last place I worked saved pdfs at every save. I got mixed up. Doing that with dxfs makes no sense.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Flat Pattern in one step

Honored Contributor
Honored Contributor

If DXF files are used to cut each part. Then there can be a huge need for it.

Betreff: Flat Pattern in one step

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

 

 

 

this is a matter of modifying the batch macro. 

 

I think, we did this a couple of years ago and so could save every flatvpattern of any psm fike within a directory structure .

 

 

Have a look into the code, setbthe filter to psm only and change the save line to saveflat pattern.

 

 

regards
Wolfgang

Re: Flat Pattern in one step

Legend
Legend

I found this via Google, sounds like it does what you're looking for:

 

http://community.plm.automation.siemens.com/t5/Solid-Edge-Forum/PSM-to-DXF-tool/m-p/309717#M12627

 

I tried it, it worked on a few, then crashed. Then my path finder display was messed up. I had to close SE, and restart fixed the issue. Seems like it's intended to work like what you're looking for, but might need a little work.

 

ST8 MP9
Go FAST, or go home.