Cancel
Showing results for 
Search instead for 
Did you mean: 

Flat Patterns not showing Gussets?

Valued Contributor
Valued Contributor

I thought when gussets first came out, the flat patterns would show deformation features like gussets. For the life of me, i can not get our flats to show special features on the flats.

 

Capture1.JPGCapture2.JPG

Nathan M. Gardner

https://www.etsy.com/people/NathanMGardner

Be sure to check out my work!!
Made in Maine Wood Carvings

2 REPLIES

Betreff: Flat Patterns not showing Gussets?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @ngardner

 

 

 

I can confirm that a gusset is not shown in flat pattern, also not in 3D PSM file.

What You will see are all the other formed features like dimples, etc.

 

But this also is true only if that option is turned on:

 

20180217_1633.PNG



regards
Wolfgang

Re: Flat Patterns not showing Gussets?

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Yes, gusset will not be shown on part after flattening part. I suggest using etch to show gusset position.

 

Here is a video about steps:

 

BR, 

Imics
http://solidedgest.wordpress.com/