Cancel
Showing results for 
Search instead for 
Did you mean: 

Flat pattern holes

Phenom
Phenom

I have a threaded hole on a sheetmetal part (ST7) for which I've set the hole geometry to be 'tap drill diameter' in the hole dialog.  However on the flat pattern draft view the hole has the thread anotated as a partial circle which will confuse the laser profiler - does anyone know a way of just showing the hole geometry on the flat pattern view?

 

holes.JPG

3 REPLIES 3

Re: Flat pattern holes

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

I suggest looking at Save as Flat DXF Options tab where you can set Complex holes exporting up. I think you should be disabling save to DXF.

 

BR,

 

Imics
http://solidedgest.wordpress.com/

Re: Flat pattern holes

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

That partial circle with only one gap is an ISO drafting standard thing whereas ANSI makes it a multi-dashed, hidden type of circle.

You could use "nominal diameter" instead of "tap drill diameter" if you don't want two circles showing.

Edit: I don't know how relevant this is to your issue or if it affects dxf output.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Flat pattern holes

Honored Contributor
Honored Contributor

The flat pattern should model the required pilot hole before the downstream operation of tapping a hole. Unless the same machine that cuts the part taps the hole. Then I'm not sure what the right thing is.

 

Isolating this kind of a step is one of my requests on a sheet metal thread.