Cancel
Showing results for 
Search instead for 
Did you mean: 

Force vertical alignment

Valued Contributor
Valued Contributor

Sorry for these basic questions, but please bear with me.  I have a simple sketch and want to align the midpoint of the base with the origin.  I select the origin and the midpoint of the base, but when I click on the horizontal/vertical relationship, it line them up horizontally.

 

How do I force a vertical alignment?  Wouldn't be easier to have separate buttons for horizontal and vertcial alignment?

 

sealign.png

4 REPLIES 4

Betreff: Force vertical alignment

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

 

 

Simply use the "Connection Relation" instead.

 

This is the upper left button in the relate area.

 

 

regards Wolfgang 

regards
Wolfgang
Highlighted

Betreff: Force vertical alignment

Valued Contributor
Valued Contributor

Thank you.

Re: Force vertical alignment

Community Manager Community Manager
Community Manager

While connect will work, the issue you were having with Vertical alignment is that you were just too far from vertically aligned to begin with. The H/V command looks at current situation and does H or V, depending on which one is already closest. So if you had dragged your shape over to be more or less under the Csys, then chosen H/V, it would have worked just fine.

Dan Staples
Director, Solid Edge Product Development

Betreff: Force vertical alignment

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Welcome,

 

 

fine if this will work.

 

regards Wolfgang 

regards
Wolfgang