Cancel
Showing results for 
Search instead for 
Did you mean: 

Foreshortened Radial Dimension

How do I create a foreshortened radial dimension that looks like this? I see the jog menu pick but I can't figure out how to shorten it enough. I've attached the draft file.

 

 

foreshortened_radial.PNG

 

 

David McMahon
Solid Edge 2019
HP Z2 Mini, Windows 10
8 REPLIES 8

Re: Foreshortened Radial Dimension

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @David_McMahon,

 

Mine seems to place OK [if my pic below, is what you want to do]......what seems to be not working for you? There are edit points that you can manipulate after placement also.

 

2016-02-25 (6).png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Foreshortened Radial Dimension

When I turn on the jog option, it inserts the jog but the center point of the radius is off of the drawing and I can't shorten it to look like what you did. How do you move the radius center point?

David McMahon
Solid Edge 2019
HP Z2 Mini, Windows 10

Re: Foreshortened Radial Dimension

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

This is all I did....hope it helps.

 

(view in My Videos)

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Foreshortened Radial Dimension

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,


Yes this could be reproduced here too!

 

Once started with a full radius dimension, changing it afterwards makes it impossible to shorten the dimension line backwards from the center.

Length is fixed to roiginal.

 

Seems to be a bug?

 

 

regards
Wolfgang

Re: Foreshortened Radial Dimension

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Ah yes, modifying a full radius dimension to be a "shortened" jogged one is different....& as Wolfgang says, this seems to be a bug.

 

Still, it's not a total deal breaker to simply delete the unwanted dim, and create the jogged radius dim again to achieve the desired result.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Foreshortened Radial Dimension

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

 

 

 

same will be true for the shortend radius dimension even if it was created shorted.

 

You can not change the length of the dimension line.

It always is keeping the line length.

 

 

regards
Wolfgang

Re: Foreshortened Radial Dimension

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

@hawcad wrote:

Once started with a full radius dimension, changing it afterwards makes it impossible to shorten the dimension line backwards from the center.

Length is fixed to roiginal.

 

Seems to be a bug?


 

Hi,

according to GTAC in ST8 it is a bug. It is fixed in ST9.

 

Ota

Highlighted

Re: Foreshortened Radial Dimension

Thanks to Sean for the workaround and everyone else that replied to this.

David McMahon
Solid Edge 2019
HP Z2 Mini, Windows 10