Cancel
Showing results for 
Search instead for 
Did you mean: 

Format Property Text - Integer function?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I am importing a property from a PDM/PLM system which happens to be the Revision.Version (Ex. "4.8").  I want to display the Revision as Property Text on my title block as "4".  I can eliminate the decimal from the Property using the "/@0" format code, but it then rounds "4" to "5" which is not what I want.  Has anyone found a way to basically get the Integer of a decimal number in Propert Text?

 

Using Variable Table is not an option as this value has to come in as a Solid Edge file property.



Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com
2 REPLIES

Re: Format Property Text - Integer function?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Ken,

 

Could that not be another character, so it is not read as an integer? I guess, in your case, your looking to "supress" it.

Seems this question is too curly for mere mortals, if you're stumped.....maybe those other matrix-reading peeps @jnewell@Tushar and @Imics have something in their bag of tricks to help.

 

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x3 seats]
Windows 10 - Quadro P2000
Testing: Solid Edge 2019

Re: Format Property Text - Integer function?

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

I don't know such format code to property text... Smiley Sad

 

In this case I do a "new custom property" from "old" and use Search and Replace function. I know this is "manually job", but I know better...

 

 

BR,

Imics
http://solidedgest.wordpress.com/