Cancel
Showing results for 
Search instead for 
Did you mean: 

Format column in parts list to show leading zero

Valued Contributor
Valued Contributor

Capture.PNG

 

i have an item in my parts list that is showing the mass as .5 kg but i want it to show 0.5kg instead. 

 

how can i change the format so that zero is show. 

 

Regards,

MagRiz
(ST9 User Est 01.18)
3 REPLIES 3

Betreff: Format column in parts list to show leading zero

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MagRiz

 

 

 

what surprises me here a little is, that when I put a mass into the BOM it always shows the leading 0 without any settings or changes.

So the question might be, wherefrom are these values coming?

Is it a custom defined property?

 

How is it defined in the 3D file?

 

regards
Wolfgang

Betreff: Format column in parts list to show leading zero

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MagRiz

 

 

... and the same seems to be true in Your BOM too.

There also the most right colum shows a mass of "0.000kg"

 

 

regards
Wolfgang

Betreff: Format column in parts list to show leading zero

Valued Contributor
Valued Contributor

Hi

It was defined as text in the properties for that part. the text field included the 0 but it wasnt pulling it through in the BOM. i have managed to find a work around by changing the decimal places from 1 to 3. so now it shows the leading 0 as 0.500. not quite 0.5 but it will do. 

 

 

Regards,

MagRiz
(ST9 User Est 01.18)