Cancel
Showing results for 
Search instead for 
Did you mean: 

Foro latino solidedge experiencias

Experimenter
Experimenter

hola, necesito ayuda, instale solid edge estudiante 9 y no corre, tengo problemas al instalarlo, tengo un PROCESADOR I3, CON 6 GB DE RAM, Y LA INSTALACION ES SATISFACTORIA, PERO NO CORRE EL PROGRAMA LO ABRO Y SE BLOQUEA, AYUDA URGENTE

4 REPLIES 4

Re: Foro latino solidedge experiencias

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @germancho,

 

Can you provide some more details of your computer system, and problem? [what Windows version, what Graphics unit & Driver version....do you have MS-Office installed?, do have you had Solid Edge loaded previously?....have you tried temporarily disabling your Antivirus program for the install?]

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Foro latino solidedge experiencias

Experimenter
Experimenter

hi Sean.

sorry, i don´t speak english.

 

windows is version 7 profesional.

service pack 1.

6g RAM.

procesador intel core i3 2.13 GHz

tis is the first installation of solid edge.

the program stop when i paint a solid ISO metric Pieza.

 in other options, the program don´t have problem.

Intel graphics media accelerator HD.

do you have teamviewer?

thanks

 

thanks.

 

 

Re: Foro latino solidedge experiencias

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there German [@germancho],

 

I used the translate page option to reveal your words, as likewise, I don't speak Spanish......so while I do have Teamviewer, I fear it would not help, as I wouldn't understand your systems localisation. I suspect your graphics may be the issue, so IF you can get to it, there may be a lesser performing setting to try.

 

Take a look at this "similar" topic for what to try [hopefully you can understand what is said there]..... https://community.plm.automation.siemens.com/t5/Solid-Edge-Student-Edition-Forum/Solid-edge-ST6-scre...

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Foro latino solidedge experiencias

Experimenter
Experimenter

hi Sean.

i'm working in the program correctly.

the problem was the graphics options, and your information is very important.

thank you.