Cancel
Showing results for 
Search instead for 
Did you mean: 

Frame Design strange drawing

Pioneer
Pioneer

Hello!

 

This problem has been here since ST10 but ony now could reproduce it on purpose.

 

When I put a frame design in drawing and set it shaded with edges then set that quality more than 150px/dpi I get the image I attached. This thing only occurs when the quality of shading is set more than 150px/dpi AND when The assembly file is not opened the same time as the drawing.

When it is and I update the drawing everything is fine.

 

Is it a bug or there is something I miss?

1 REPLY 1

Re: Frame Design strange drawing

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Reseter  BUG.  Log it with your VAR.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com