Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Frame Miter angle not showing

Valued Contributor
Valued Contributor

I have a 1" tube frame for an awning I am making.  I have a cut list with the end miter angles included.  However, for some reason on this assembly it is NOT populating the miter fields.  Please help.

 

Capture.JPG

3 REPLIES 3

Re: Frame Miter angle not showing

Siemens Phenom Siemens Phenom
Siemens Phenom

Without deep diving, this currently cannot be accomplished and is an existing ER.

 

I would suggest submitting the file to your local support resource for further investigation at which time you can be added to the existing ER.

Re: Frame Miter angle not showing

Valued Contributor
Valued Contributor

Ive had it to it before, its just not working on the particular assembly.  see here is another assembly it pulls in the miter angles from.  Miter Angle 1 & Miter Angle 2 are selectable columns and data you can pull into cut lists

 

Capture2.JPG

Betreff: Frame Miter angle not showing

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @lifofadrafter

 

 

 

I only can do an assumption what could be happend here.

 

How are those frame elements created?

Are the ends possibly trimmed rather than created in native frame manner?

 

If trimmed You never ever will get any miter angles.

 

regards
Wolfgang