Cancel
Showing results for 
Search instead for 
Did you mean: 

Frame Sequence Position Change in the path Finder

Experimenter
Experimenter

Hello All,

I am creating tube runs using Frame function and i would like to change the sequence of frame components as per my need which helps manufacturing/assembly. But Frame is not allowing me to change the sequences.

 

If you refer the attachment, there are three frame (Frame 11,10,13) and i want to move the frame 13 to be ahead of Frame 11.

Please help how can i do this.

1 REPLY 1
Highlighted

Re: Frame Sequence Position Change in the path Finder

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there,

 

AFAIK, frame cannot be reordered like you would expect an "Ordered Mode" feature tree would do. We find that this is usually just as fast, if not more so, than conditional editing.

Without inspecting the model issue, you will most likely need to delete the incorrect elements and recreate them in the order you need, to get the desired outcome.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP7] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000