Cancel
Showing results for 
Search instead for 
Did you mean: 

Frame, draft, Tube Flat Length is empty

Hi,

 

Why is the value of "Tube Flat Lenth" always empty for me when making a draft of my frames?

What am I missing?

 

Hope one of you might be able to help me Smiley Happy

 

 

Thanks,

Kenneth

5 REPLIES 5

Re: Frame, draft, Tube Flat Length is empty

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Maskinbyggerne  Not certain, but I was thinking Tube Flat Length was for XpressRoute created tubes, not Frame components.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: Frame, draft, Tube Flat Length is empty

 

 

Ahh, I did not know that.

I can see that "Cut Length" is working Smiley Happy

 

Thanks,

 

Re: Frame, draft, Tube Flat Length is empty

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Maskinbyggerne

 

 

 

Cut Length is one property for Frames but there also the Total Length is available for them, adding together the length of the same profile types.

 

regards
Wolfgang

Re: Frame, draft, Tube Flat Length is empty

Thank you very much for that info Smiley Happy

Re: Frame, draft, Tube Flat Length is empty

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Maskinbyggerne

 

 

 

welcome, and I also would like to have one single property for tube/frame length if there are pipes and frames in the same assembly.

At the moment You need two different props/columns in BOM to show those item length values.

 

 

regards
Wolfgang