Cancel
Showing results for 
Search instead for 
Did you mean: 

Free 2D ST10 availablility

Legend
Legend

We use on some workstations Free 2D  (purchasing, etc)

 

Is there anyone who knows when this license / download becomes available..

 

Kind regards,

 

 

Jan Bos

 

13 REPLIES 13

Re: Free 2D ST10 availablility

Legend
Legend

It already is, when you install ST10 and when it asks for licence you can select the bottom one. That says use only 2D draft or something which is free and you don't need licence for that.

 

Good feature if you ask me.

 

So no extra downloads needed, just install ST10.

Sander
The Netherlands

Re: Free 2D ST10 availablility

Legend
Legend
Thanks, bedankt..

Perfect will give it a try tomorrow,

Thanks,

Jan

Re: Free 2D ST10 availablility

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @Jan_Bos,

 

A word of warning however, as in a recent blog post  comment by Alard [@edobp016], for higher level users, changing the licensing "down" to 2D only, overwrites the existing license file that way. So you would need to restore it from a backup copy, to return full functionality.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Free 2D ST10 availablility

Siemens Phenom Siemens Phenom
Siemens Phenom

FYI, for non-Solid Edge customers, the ST10 Solid Edge Viewer (which is full Solid Edge with the Free2D/Viewer mode enabled) can be downloaded from here:

 

https://www.plm.automation.siemens.com/en/products/solid-edge/freeviewer/index.cfm

Re: Free 2D ST10 availablility

Creator
Creator

Good day,

This not so much a reply, more a similar question.  Is Free 2D ST10 available in the UK yet?  On the download page selecting 'United Kingdom' in the required address details page defaults back to 'United States'.

 

Sincerely,

Roger

Re: Free 2D ST10 availablility

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @RogerH,

 

Using @uk_dave's link above to the download sign-up page, choosing UK sticks OK for me. [although, I'm not in the UK]

 

Maybe try using a different browser?

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Free 2D ST10 availablility

Creator
Creator

Sean,

Many thanks - using a different browser sorted the problem.  The download went smoothly, I had a bit of an issue with the licence.  The solution is easy, as another contributor mentioned, it is the final radio button on the 'drop down' list. 

 

Unfortunately, theprogramme crashes when opening files with a message along the lines of 'the program will have to close.'  I guess this means re-installing but perhaps there are other suggestions?

 

Sincerely,

Roger

Re: Free 2D ST10 availablility

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @RogerH

 

 

 

have You downloaded the Maintenance Pack2 for ST10?

 

This would be the first I would try

 

regards
Wolfgang

Re: Free 2D ST10 availablility

Creator
Creator

Good evening Wolfgang,

Goodness, that was quick!  I have the free 2D version of ST10, is Maintenance Pack 2 appropriate for this version?

 

Sincerely,

 

Roger