Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Free Macro - Show or Hide Surfaces

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

This little app toggles the display of the surfaces generated by the Extract command on the Reverse Engineering tab on the ribbon bar.

Background and usage:

When you bring in scanned data into Solid Edge in the form of an STL file, the Automatic command on the Reverse Engineering tab colors the various regions and further the Extract command creates various types of surfaces automatically, in huge numbers:

1. Planar
2. Spherical
3. Conical
4. BSpline
5. Cylindrical

It becomes cumbersome to show/hide these surfaces manually, specifically when you want to hide all surfaces of one type, say Spherical, or just the BSpline surfaces.

 

 

This free macro helps you quickly toggle the display of each type of surfaces with one click.

http://www.surfandcode.in/2019/01/solid-edge-app-show-or-hide-surfaces.html

2 REPLIES

Re: Free Macro - Show or Hide Surfaces

Gears Phenom Gears Phenom
Gears Phenom

Thnx, brilliant!

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Free Macro - Show or Hide Surfaces

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Thank you @Imics Smiley Happy