Cancel
Showing results for 
Search instead for 
Did you mean: 

Free Solid Edge Capture Screen tool

Gears Phenom Gears Phenom
Gears Phenom

 

The Solid Edge Maker Faire offers a free Capture Screen tool for Solid Edge.

The program and source code can be downloaded from this link.

 

00.png

 

This utility can be run from within Solid Edge Part, Assembly and Sheetmetal via a button on the ribbon and captures just the model view to the clipboard.

 

After pressing the button, no further action is required. You can immediatly paste the image from clipboard to your editing program or instantly open the image file that is automatically created by this tool.

 

Unlike other screen capturing programs, you don't have to explicitly specify the Solid Edge graphics window to capture the model image. This tool does it automatically.

 

~Tushar Suradkar

www.SurfAndCode.in

 

10 REPLIES

Re: Free Solid Edge Capture Screen tool

Gears Phenom Gears Phenom
Gears Phenom

Thank you for your effort! Smiley Wink

Imics
http://solidedgest.wordpress.com/

Re: Free Solid Edge Capture Screen tool

Gears Phenom Gears Phenom
Gears Phenom

Thank you Imi for the kind words, these help me keep going Smiley Happy

 

Re: Free Solid Edge Capture Screen tool

Phenom
Phenom
Thanks Tushar!

Very helpful application.

The next step could be to be able to capture an area from the hole picture Smiley Happy

Yasser

Re: Free Solid Edge Capture Screen tool

Gears Phenom Gears Phenom
Gears Phenom

Thanks Yasser,

I accept the challenge hole heartedly Smiley Happy

 

~Tushar

Re: Free Solid Edge Capture Screen tool

Gears Phenom Gears Phenom
Gears Phenom

Hello,

 

I'll definitely give this a try.

 

For a lot of situations, I use the snip tool found in windows.  It's really handy, but having a program inside SE is even better.

 

Kyle

Kyle Joiner
IPA LLC
ST10 MP1

Re: Free Solid Edge Capture Screen tool

Pioneer
Pioneer

I use Snagit myself as it provides a number of good tools

Re: Free Solid Edge Capture Screen tool

Phenom
Phenom

Tushar-

This is a nice add-in /app for SE on pc.

 

As for me, I like SE on the Surface Pro 3. I just double click on the head of the sytlus and drag window around my area and volia I've got my area captured and ready to share with just about any application that will take a paste function. In my case, I paste the image into a OneNote Design Review template I created and start marking things up. :-)

Re: Free Solid Edge Capture Screen tool

Gears Phenom Gears Phenom
Gears Phenom

I love: 

http://getgreenshot.org

to take screenshots and

http://www.techsmith.com/jing.html and http://www.bbsoftware.co.uk/BBFlashBack/Home.aspx

ta make video's.

 

The youtube button in SE works fine, but when you try to make a video of SE freezing, this won't work.

...........................................................................................................
Solid Edge ST10 & AutoCAD 2019 user

Re: Free Solid Edge Capture Screen tool

Gears Phenom Gears Phenom
Gears Phenom

Lightscreen was my favorite until I discovered that Greenshot additionally has a built in Editor which Lightscreen lacks.

One of my colleague swears by Greenshot so I will definitely give it a try. The editor UI looks similar to Paint.Net, another freeware for image editing.