Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Full ST9 and ST9 Free2D on same PC

Phenom
Phenom

Similar to @hawcad I wrote this because we didn't have enough Premium licenses for everyone.

It copies the required one to the preferences folder then starts Solid Edge.

 

LICENSE MANAGER.JPG

HP Z420 16GB RAM
Quadro K4000
SE2019 MP5 on Windows 10 Pro 64.

Re: Full ST9 and ST9 Free2D on same PC

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Edgers,


if it can help I will upload the script I'm using

 

Please have first a look into and change the pathes and file names appropriate to Your situation

 

There are the differnet license type files at the same folder as this script is.

 

Then I have a linked copy to that script onto my desktop modifying the command line with the additional word like "Premium" in the picture.

 

So You can use one and the same script file for all variaties of license types You need.

 

20170412_1649.PNG

 

After testing You can delete the "pause" command in the script

 

Hope it can help

 

regards
Wolfgang

Re: Full ST9 and ST9 Free2D on same PC

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Edgers,


i just have modyfied and updated my old SE_Version macro
and I would like to share it here fore everybody who can use it.

 

This how it looks like:

 

20170413_1453.PNG

 

 

After starting the macro will read out the "Preferenes" path of the current Solid Edge version as destination folder. Furthermore it will find all xxxx.dat files in the macro folder itself and put them on the list.

Clicking one list entry will copy those file into the preferences directory

 

So now You easily can change Your available license types with one single mouse click

 

Hope it helps and saves time!

 

 

 

regards
Wolfgang

Re: Full ST9 and ST9 Free2D on same PC

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Edgers,

sorry for another psot, but I have modyfied the macro again, so that a double-click on the bottom text field (showing the current location of the license) will open it and show the content within a text box.

This came up by myself for easier control the current content.

This saves me from opening the explorer, changing to the prefrences folder and open the SELicense.dat.

 

Hope You can use it.

 

regards
Wolfgang