Cancel
Showing results for 
Search instead for 
Did you mean: 

Fun problem solved

Honored Contributor
Honored Contributor

I have been going through some major growing pains moving from one use too two users on a server.

 

One of the problems we ran into was that when my computer has handed to another user, that user could not edit materials.

 

The solution was to delete all of the registry entries. This worked because the problem was the screen location of the materials. The old user had a high resolution screen, the new user did not. So the material menu was showing up off the screen. We had no idea that was going on.

 

I hope others can benefit from this.

3 REPLIES

Re: Fun problem solved

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Did you not think of changing the screen resolution to a higher value if possible to get the floating dialog back into view.

Not saying that I fully understood what the problem was with the material dialog or that the aforesaid method would have succeeded in your case, but have used this trick before for getting floating things like the Command Bar back into the visible area of the screen.

Re: Fun problem solved

Valued Contributor
Valued Contributor
Some nvidia drivers using nview allow you to force things opening off screen to be opened on the main screen. I may not have explained that very well! could be useful.

CAD/CAE Manager
ST8 MP12

Re: Fun problem solved

Honored Contributor
Honored Contributor

The computer was moved from one desk to another. The new desk did not have monitors that could handle 4K resolution. Was not an option. DVI vs Display port inputs on the monitors.