Showing results for 
Search instead for 
Did you mean: 

Get Set Go


If you often work with a specific set of files and want to open the last closed bunch quickly, Get-Set-Go for Solid Edge will come in handy and make the process easy and streamlined.




If files are open in Solid Edge, they are all listed in the dialog. You can then save this set of files to a .SET file.

The same set of files can be later opened from the Load Set button and the files are listed back in the dialog. You can further check-uncheck files from this list and open only the checked files in Solid Edge using the Open Checked Files button.

While Get-Set-Go is still running, files can be manually opened or closed in Solid Edge. Click the Refresh button to reflect this new set of open files in the dialog.
The new set can then be again saved as a different .SET file using the Save Set button.


Direct download from this page, contains Readme PDF, the EXE and a PNG for the Solid Edge button or Quick Access icon.


Watch a video here.


~Tushar Suradkar