Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Getting the length of imported bent pipe

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Does anyone have any ideas on how you can get the centerline of a piece of (imported) bent pipe and then hence the length?

4 REPLIES 4

Re: Getting the length of imported bent pipe

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If the pipe lies on a single plane then it's pretty easy. If it's on multiple planes then it gets more difficult. Haven't run into that issue so I'm not sure how I'd approach it.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Betreff: Getting the length of imported bent pipe

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Alan 

 

 

 

there was the same question last week, or at least for me it sounds as being the same.

 

"How to get the length of an imported pipe"

 

I have added a video there.

Here under android I'm not able to copy the link to that post.

But just scroll back to last weeks items.

 

 

regards
Wolfgang

Betreff: Getting the length of imported bent pipe

Solution Partner Legend Solution Partner Legend
Solution Partner Legend
Thanks @hawcad

Betreff: Getting the length of imported bent pipe

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Alan 

 

 

welcome.

I just came back to the office and was going on to provide the proper link or the video, but it seems, that this is not necessary any more.

 

 

regards
Wolfgang