Cancel
Showing results for 
Search instead for 
Did you mean: 

Glue Connectors not 'gluing'

Experimenter
Experimenter

Hello,

 

I am relatively new to using SolidEdge / CAD packages.

 

I have a question regarding the glue connectors used in the SolidEdge student edition.

 

Essentially I have a cylindrical-like solid between two posts and I want to apply a strain to this cylinder by displacing one of the posts whilst one of the posts remains fixed.

 

I have defined the left hand post to be fixed and the right hand one to move 1.5mm along the x axis as so:

 

Construct.jpg

 

 

I have then connected both posts (one at a time) to the cylinder by simply using the auto connector glue tool and selecting the post followed by the tendon:

 

Connectors.jpg

 

When I look to run the simulation e.g. solve, everything seems to work well apart from the cylinder pulling away from the post at either side. See below - a gap forming between the post and the cylinder (picture shows this particularly on the right hand side but this is also happening on left hand side)

 

Simulation.jpg

 

How am I able to create a 'secure' tight connection between both the post and the cylinder which does not move apart if the glue option is not doing this?

 

Thanks,

 

Richard 

 

 

 

 

 

 

1 REPLY

Re: Glue Connectors not 'gluing'

Valued Contributor
Valued Contributor

Is there a gap between the respective mating faces that you want glued together?  Are all there parts solids or surface bodies?