Cancel
Showing results for 
Search instead for 
Did you mean: 

Goal seek wont make a Dimension 0 ?

Pioneer
Pioneer

Hello guys,

 

                  I am trying to make an assmebly of chain links.

I added all parts manually and constrained them as pattern along curve wanst giving the expected result

However i am not able to constrain the last link as the axial aling wont work due to a small difference.

I tried using goal seek but it isnt working.

I have attached the assembly. The dimension i want to be 0 is Linear_1.

Any help in this regard is appreciated.

 

Thanks,

Balaji

9 REPLIES 9

Re: Goal seek wont make a Dimension 0 ?

Phenom
Phenom

I doubt whether 0 would be possible, but try 0.0000001

HP Z420 16GB RAM
Quadro K4000
SE2019 MP5 on Windows 10 Pro 64.

Re: Goal seek wont make a Dimension 0 ?

Pioneer
Pioneer
The whole point of making it 0 is because i want to axial align it.
even if it comes down to 0.0000001 it wont axial align right?

Re: Goal seek wont make a Dimension 0 ?

Phenom
Phenom
I see your point, but no it will not axial align.
Maybe 0 is not a permitted value, but how about placing a fixed point or line say 10mm away from the origin point of your dimenson and then dimensioning back to the point you are moving.
HP Z420 16GB RAM
Quadro K4000
SE2019 MP5 on Windows 10 Pro 64.

Re: Goal seek wont make a Dimension 0 ?

Pioneer
Pioneer

Thank you for your reply @beachcomber

 

I am not able to move it exactly 10mm away either not sure what i am doing wrong.

Tried  goal seek too but wont work for some reason. 

Re: Goal seek wont make a Dimension 0 ?

Legend
Legend

It doesen't work in your case, because the logic won't recognize the difference of the +/- direction of your dimension. Put a dimension from one chain link to the other on from the same end. The dimension is 84.XX and the make a search with the target 85.00. I had to increase the time limit from 60s to 120s to make it work.

Greetings from Germany
Christian Kunkel
https://c-k-m.info

Re: Goal seek wont make a Dimension 0 ?

Phenom
Phenom

@ckunkel72 That was the kind of thing I was suggesting - it just needs a 'real' dimension to work to, so I would think any dimension to a fixed point will work (given time)

HP Z420 16GB RAM
Quadro K4000
SE2019 MP5 on Windows 10 Pro 64.

Re: Goal seek wont make a Dimension 0 ?

Pioneer
Pioneer

Thank you @ckunkel72 for your reply.

 

I tried as you said my dimension became 85.00XXX and after goal seek although it was solving unlike before

the value i am getting is still 85.XXXX or 84.999XX.

The closest value i got is 85.000046

Still cant get it to axial align.

After you solved it could you axial align it ?

Re: Goal seek wont make a Dimension 0 ?

Phenom
Phenom
The goal seek is an iterative process, so may require hundreds of calculations to solve.
I would suggest not worrying about the axial align and use different constraints.
HP Z420 16GB RAM
Quadro K4000
SE2019 MP5 on Windows 10 Pro 64.

Re: Goal seek wont make a Dimension 0 ?

Pioneer
Pioneer

yes @beachcomber i guess i will hhave to use other constraints.

After several attempts the best value i could get is 85.000009.