Cancel
Showing results for 
Search instead for 
Did you mean: 

Google Sheets

Valued Contributor
Valued Contributor

Can I embed google sheets into a Solid Edge draft?

8 REPLIES
Highlighted

Betreff: Google Sheets

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @mezcofab

 

 

sorry for this question from an old "dino".

 

But what is a "Google Sheet"?

This is essenstial to know for answering the question "How do ...?"

 



regards
Wolfgang

Betreff: Google Sheets

Siemens Phenom Siemens Phenom
Siemens Phenom

Google Sheets is Google's spreadsheet program.

 

No, you cannot embed the Google Sheets data as a table into Solid Edge.  You can only do this with Microsoft Excel.

 

You could theoretically save the Google Sheets file to disk and then embed the file into Solid Edge but I suspect that is not what you are looking for..  

Betreff: Google Sheets

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @uk_dave

 

 

 

thanks You very much for let me learn "my today's new"

So this day became a good day.

 

Now I know exactly what the original question was, but I wasn't samrt enough to knwo that this is named Google Sheets

 

 



regards
Wolfgang

Betreff: Google Sheets

Valued Contributor
Valued Contributor

I created a time collection spread sheet and I wanted to embed it in my draft for quick access. If I export it to an excel format it takes out the script I created in google sheets.

 

Thank you for the answer.

Betreff: Google Sheets

Valued Contributor
Valued Contributor

I was able to connect a hyperlink to an entity to direct me to the google sheet.

 

Attached is screenshots and sample.TEST DRAFT.pngPUNCH CLOCK.png

Betreff: Google Sheets

Genius
Genius
+1 for a Google sheets user. I avoid Excel....

Betreff: Google Sheets

Gears Phenom Gears Phenom
Gears Phenom

mezcofab wrote:

I was able to connect a hyperlink to an entity to direct me to the google sheet.


 

I had the same idea of linking to a online sheet, but then your question said 'embed' which would not be the same.

Betreff: Google Sheets

Phenom
Phenom

If one of the reasons you're asking is because you don't have or want to pay for MS Office, another option is to sync the spreadsheet to the cloud with OneDrive or Dropbox and use the (free) MS office online tools which is built into both those services to edit it in a browser.  

 

The end result is that you're using a MS Excel sheet which suits SE, without having to have the applcaition installed locally.

 

Obviously if you're stuck with google sheets for whatever reason, that's another story.