Cancel
Showing results for 
Search instead for 
Did you mean: 

Gradient Background Override not sticking

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

We've notice today that if you choose Gradient as a background ground it doesn't stick. next time you do a new par, or assy. It's defaults back to solid??? anyone else notice this?

4 REPLIES 4

Re: Gradient Background Override not sticking

MLombard
Retired

This is a document based setting, so you have to save it in a template, and use that template for new documents to get the setting.

Retired Community Manager for Solid Edge. This account is no longer active.

Re: Gradient Background Override not sticking

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Keep in mind that the gradient background affects the thumbnail that is created at save and the thumbnails usually are undecipherable when created using a gradient background.  Also, every poor soul who opens the file has to see the gradient background until they change it since it is saved with the file.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com
Highlighted

Re: Gradient Background Override not sticking

Phenom
Phenom

We have a gradient background in our template and the thumbnails are fine. It's probably because there's a good contrast between the part colours and the background - maybe the default black/white in the std templates isn't as good.

gradient.png

Re: Gradient Background Override not sticking

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

That's just it.  With most parts being the light gray by default and most users using the black to white gradient, you end up with shades of gray right where the model is and it's hard to see what the detail is in the thumbnail.

 

Now if the background was not gradient but instead was a lighter solid color like light gray, SE automatically makes the background white when it creates the thumbnail. If it is a darker background it makes the thumbnail background black.  White provides great contrast and works well in most UI's that display a thumbnail, for instance Windows Explorer.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com