01-30-2018 07:02 AM
Hi,
I have a graphic problem in assembly.
When I have an open assembly, and passes over a part, the assembly dissapears.
I attach a video
Any suggestions on what may be happening?
Best regards,
Xènia Turon
Solved! Go to Solution.
01-30-2018 08:13 AM
01-30-2018 08:45 AM
Hi @hawcad,
I have a Dell Precison T7500 with Windows 7 Professional.
Intel(R) Xeon(R) X5650 - 12 GB and 64bits
NVIDIA Quadro 600
01-30-2018 09:05 AM
Hi @xeniaturon
OK, win7 and nVidia 600
Is it correct, that the 600 is a more or less smaller graphic ard, but should do its job anyway.
What settings have You set in Solid Edge options for the Graphics?
01-30-2018 09:27 AM
01-30-2018 09:30 AM
Hi @xeniaturon
try to change the Automatic Graphic Selection to manual Graphics Card Driven (no Advanced)
Stop SE, Start again and see what happens.
01-30-2018 09:31 AM
Hi @xeniaturon
before changing check the Applications Graphic setting, wether the Quadro 600 is fully dedicated to Solid Edge.
You said this is a notebook, and normally they have an onboard graphic too.
Maybe here is a difference which one should be used.
01-30-2018 09:59 AM
01-30-2018 10:07 AM
Hi @hawcad
after changing to manual Graphics Card Driven it works better but when selecting parts it does not look quite right.
It would be an interim solution.
Thank you.
Best regards,
Xènia Turon
01-30-2018 10:17 AM
Hi @xeniaturon
so I would work on the graphics driver and graphics settings to improve the behaviour and performance