Graphics Settings for ST7 -Nvidia Quadro K5000

Pioneer
Pioneer

I need some help in graphics settings for Solid Edge ST7. 

I feel that the display what I am getting in assembly could be of more superior quality with my Worstation Configuration.  I tried with many option but couldnt improve it. I guess something is wrong with Anti-Aliasing. Am I missing something? Please Refer images. 

Please help. 

 

 

My Workstation Configuration : 

FUJITSU, CELSIUS M730power

Intel(R) Xeon(R) CPU E5-1650 v2 @ 3.50GHz

32GB RAM

NVIDIA, Quadro K5000, 9.18.13.4817

Display: 1920x1080x32 @ 60Hz

Windows 7

 

With Anti-Aliasing.jpgWith Anti-Aliasing.jpgSE View Setting.jpgNvidia Adjust Image.jpgNvidia Manage 3D.jpg

5 REPLIES

Re: Graphics Settings for ST7 -Nvidia Quadro K5000

Phenom
Phenom

I got an old Quadro FX1800 and I get great result with this settings:

 

quadro.png

Re: Graphics Settings for ST7 -Nvidia Quadro K5000

Pioneer
Pioneer
Thanks Fiorini,
I tried with these setting but there's no change.

Re: Graphics Settings for ST7 -Nvidia Quadro K5000

Phenom
Phenom

What sort of improvements are you looking for? I have the same card and my display looks the same.

 

The display of the parts will be mostly defined by the materials/face colours etc. that you apply to them so if the parts don't have textures or bump maps etc. applied they will just have a plain colour whatever the settings are.

Re: Graphics Settings for ST7 -Nvidia Quadro K5000

Pioneer
Pioneer

The display can be much better than this. We still have ST2 . I have attached few images from ST2 which is installed on much lower configuration than mine. I have set the Antialias level to high. 

 

Issue is that the edges are not crisp and clear. 

 

Re: Graphics Settings for ST7 -Nvidia Quadro K5000

Valued Contributor
Valued Contributor

Thanks mate it worked for me! I have a lenovo p50 with Nvidia Quadro M2000M.

 

Good luck