Cancel
Showing results for 
Search instead for 
Did you mean: 

Graphics issue -- Windows 7

Experimenter
Experimenter

Hi all,

 

I'm new to Solid Edge and have an annoying problem. New features (if that's the right word) have these contrail-like afterimages that only disappear after I've placed the feature or selected a new tool. I need a solution, because this makes careful work difficult. There should be a picture appending this post showing my problem.

 

 Some information about my computer and program:

I'm using a mid-2010 iMac with 8 gb RAM and an AMD Radeon HD 4670 graphics card. I'm running Windows 7 Professional installed on a partition created with Boot Camp. I have Solid Edge 10, with maintenance pack 8 installed. 

 

I've tried installing drivers for my graphics card and for Boot Camped Windows 7 and neither fixed my problem. Any help would be appreciated.

2 REPLIES 2

Re: Graphics issue -- Windows 7

Gears Phenom Gears Phenom
Gears Phenom

You need to change some settings in Options- View

 

Untick the Automatic selection and choose Graphics Card driven (Basic)

 

opzioni visualizza.png

Betreff: Graphics issue -- Windows 7

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @sleepyscribe

 

 

 

besides the settings mentioned by @Fiorini I only must say that this type of problems I have seen so much often when AMD Radeon cards are involved.

This might be the reason too that I promised myself to never ever use an AMD card in any of our computers.

 

 

regards
Wolfgang