Cancel
Showing results for 
Search instead for 
Did you mean: 

Groove welds intersecting issue.

Legend
Legend

Anyone have any idea how I can make this weld work out to what one would expect?

 

Yes welds are required and the bevels are required.

 

https://www.youtube.com/embed/LDW5NumVeOg

 

 

Solid Edge ST7 MP10

3 REPLIES

Re: Groove welds intersecting issue.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @nanan00,

 

Can you not model the required full weld volume and then assign it as a weld afterwards?

 

 

See this ST6 video from @Imics....

 

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Groove welds intersecting issue.

Legend
Legend

If it was just one corner I would do that but it is in about 10 places.

 

The stuff we build has hundreds to thousands of feet of weld and I need to be able to show details of tricky areas.

 

I have also run into problems with the fillet welds working fine in 3 places but not the 4th on mirror placed patterns of parts...

 

Does anyone know how to set the fillet weld option to a default weld? I want equal setbacks with a .375 base thickness and it keeps resetting to bisector of .25...

Re: Groove welds intersecting issue.

Legend
Legend

Pic one, a fillet weld wrapped around the intersection of a flange and a rib, works as intended.

 

Pic two, mirror side of part, copy of original flange and rib with exact same relationships etc. Can not get the weld to wrap completely.

 

Pic three, if the back side of the flange and rib are left out the weld completes. A second weld was tried to get the backside of the flange and rib. Was unable to include any other faces in any combination to make the wraparound at least look halfway not like crap.