Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

HATCH STYLE

Not applicable

I've named a few custom hatches when in my custom template file. However, when I
select the HATCH command in files that use that template, those named styles do
not show up in the drop down menu. But when I open the FORMAT/STYLE/HATCH, they
do show. Why aren't they available in the drop down menu? I set a custom DIMENSION
style and it shows when I select the DIMENSION command.
Thanks
Ron
Ronald W Latour
1 REPLY 1

Re: HATCH STYLE

Not applicable
Ron,
Good question.
Hatch styles are not used directly. Hatch styles provide the pattern
associated with a fill style. Fill is what you put into a closed area. Look
at the fill styles provided with 2D Drafting. Notice that they have an
associated hatch style. One thing that may make this confusing is that they
use the same name. Normal fill will have a Normal hatch by default.
You have created new hatch styles. Now create new fill styles and apply your
new hatch. Once you have the new fill styles created they will show in the
drop list.
Regards,
Rick B.