Cancel
Showing results for 
Search instead for 
Did you mean: 

Hack for increasing pulldown list length?

Creator
Creator

I'm wondering if there is away to increase the length of pulldown lists. I have a bunch of presets for various tables and callouts. But I wind up doing a lot of scrolling to get to the item I want. Can the length of of these pulldowns be extended? Maybe by registry key or somewhere else?

 

LIST LENGTH.png

1 REPLY 1

Betreff: Hack for increasing pulldown list length?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @RiffRaff

 

 

 

I do not think that there is an entry to define the length of list forms in SE.

 

The only "help" I can advise is to use the first characters of Your list item to fast jump to them.

 

So - for example  if You have an entry, let's name it "K-Bom" which actually is the 10th in the list, then entering a "k" will go directly to the first item beginning with a "k".

 

But maybe thee are hidden secrets of SE which will allo w to extend the length of such lists, or also to define the width of them.

Sometimes they are also not wide enough to show the full item names.

 

 

regards
Wolfgang