Cancel
Showing results for 
Search instead for 
Did you mean: 

Harness WIzard

Hi Everyone,

 

When I'm entering Harness Environment, there will be function for wire harnesss wizard. And it need 2 documents to be inserted which are 

1) Component document (*cmp)

2) Connection document (*con)

 

How to create those file documents?

 

ST9 Premium User

Window 10

2 REPLIES 2

Re: Harness WIzard

PLM World Member Legend PLM World Member Legend
PLM World Member Legend
These files should be created by an electrical schematics application such as Mentor Graphics or Cimteam. You do not have to have the files to model a wire harness. You can manually connect wire paths to connectors.

Jason

Re: Harness WIzard

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

As stated in a reply those files typically are exported from a 3rd part ECAD system and imported to Solid Edge using the wizard.  If you know the format you can use any text editor to create your own.  The format is defined under the Solid Edge\Program\Preferences subfolder using the file SEHarness.txt file. That tells you the formats for each ECAD system and is editable as well. 

Thanks
Ronnie Conerly
Product Manager, Solid Edge