Cancel
Showing results for 
Search instead for 
Did you mean: 

Hatching unselectable in "Draw in in View".

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

I have a drawing view in which I wish to edit the hatching because the spacing is too coarse.  So I go into "Draw in View" and find that no matter what I do I cannot select the hatching in order to change the Spacing.  I can select some of the hatch regions but not all of the hatch regions.  Therefore I am forced to leave the default "schoolboy" hatching intact and it looks like crap.  See attached.  This is with ST6 MP14.  This problem is a bit random and crops up just occasionally - but is still a pisser.  Is it just me or do you get this problem as well?

5 REPLIES 5

Re: Hatching unselectable in "Draw in in View".

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Chris,

 

Could it be a matter of hovering and waiting for quick pick, to then select the desired region?

Maybe the boundary is obscured by other geometry...?

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Betreff: Hatching unselectable in "Draw in in View".

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

 

 

whats about going to view properties, pathfinder view and selecting the middle part.

There should be the hatching properties on the right side of the form.

 

As far as I remember this came into SE before ST6.

 

 

I have no SE available at the moment (tablet)

 

 

regards
Wolfgang

Re: Hatching unselectable in "Draw in in View".

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

Hi Sean,

 

I had been hovering over this thing like a micro-manager and absolutely not a sausage.  However, I noted you comments about the boundary and hovered on over there.  Sure enough I was able to QuickPick the internal region.  So thanks for that!

 

Cheers,

 

Chris

Highlighted

Betreff: Hatching unselectable in "Draw in in View".

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

Hi Wolfgang,

 

I never thought of that.  Although probably not the workflow I would use much as it is easier to tweak things directly in the view.  But thanks for that!

 

Cheers,

 

Chris

Betreff: Hatching unselectable in "Draw in in View".

Legend
Legend
I never thought of that, I'll have to try it!
Using SE since V12, 2002
ST10 certified