Cancel
Showing results for 
Search instead for 
Did you mean: 

Betreff: Having trouble laying out a pattern.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @astrixkid

 

 

 

Yes, sorry, of course this is a ST10 file which will not open under ST9

 

But using the PatternByTable function still will work there too.

 

 

regards
Wolfgang

Betreff: Having trouble laying out a pattern.

Pioneer
Pioneer

I have now updated my software to ST10!

Thank you for all your help guys.

I have managed to draw the part that I needed too. Next step is to put it into my CAM programme and machine it.

I will post pics as I go along.

 

Thanks again,

 

Jim :-)

Betreff: Having trouble laying out a pattern.

Pioneer
Pioneer

As a follow on from the posts above.

 

These are the plates I am making. Thanks for all the help!

Betreff: Having trouble laying out a pattern.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @astrixkid

 

 

great, but do You have placed them now all in the same direction, different to the original intend?

 

 

regards
Wolfgang

Betreff: Having trouble laying out a pattern.

Pioneer
Pioneer
Ran some initial tests with the pressed portions of fish going down the conveyor belt and the ones that were travelling tail first crossed the transfers better without rotating giving better presentation into the fryer.

Its technical stuff frying fish :-)

There are another 6 or 7 sizes to do yet so I will post pics when done!