Cancel
Showing results for 
Search instead for 
Did you mean: 

Helix Help...

Experimenter
Experimenter

Hello,

 

This is my first time posting maybe if someone would be able to help.  I am trying to create a helix profile of the following part, but with no luck!

 

We would be using a ball nose endmill starting at one point and exiting at the second point, with a smooth transition between points and revolving the part axis.  Everytime i try it out its either not a smooth profile or it has a weird shape.

 

Regards,

Elvino

4 REPLIES

Re: Helix Help...

i had a similar challange years ago

 

this thread may be of value to you challenge as well:

 

http://community.plm.automation.siemens.com/t5/Solid-Edge-Misc/How-would-you-model-it/td-p/220555/hi...

 

Re: Helix Help...

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

oops! that link is out of bounds for some.

 

Re: Helix Help...

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

This is a tipical "volume based" sweep cutout!

 

Here is an solution what, is a good approx:

 

Hmmm, this should be an exact solution:

link (opening it only for your risk Smiley Very Happy Smiley Very Happy Smiley Very Happy )

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Helix Help...

Experimenter
Experimenter

I want to thank everyone for the links and help on trying to figure this out.  I will give it a try and work at it till i am OK with it.

 

Regards,

Vino