Cancel
Showing results for 
Search instead for 
Did you mean: 

Help: Housing Construction

Experimenter
Experimenter

Hello there,

 

I hope i am in right Forum for this question.

I am using Solid Edge ST7 and not really used to it.

I started with the contour flap and want to add a single flap.

Now the problem is - How can i make them "together".

Will add 2 pictures for an example. (Should look like the 2nd picture)

 

I hope someone can help me quite fast. appreciate it a lot.

 

Best regards,

Ramon

11 REPLIES

Re: Help: Housing Construction

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Your second picture doesn't seem to represent a sheet metal part so I wonder why you are using the sheet metal environment.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Help: Housing Construction

Experimenter
Experimenter

Does this really matter ? I mean i should be able to make it work in a sheet metal part aswell am i not ?

Re: Help: Housing Construction

Gears Phenom Gears Phenom
Gears Phenom

You can make your part in sheet metal, weld it and add a fillet.

...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user

Re: Help: Housing Construction

Experimenter
Experimenter

Is there no easy solution - like saying -> Left wall connect Right wall and add a Fase ?

 

Re: Help: Housing Construction

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I don't know but I think I'd start with a part. Make a block of the overall, draft on two sides, thin wall it, add the two flanges, a cutout and then add fillets.

 

ramon1.JPG

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Help: Housing Construction

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Joris, what do you mean "weld it"?

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Help: Housing Construction

Gears Phenom Gears Phenom
Gears Phenom

something like this

...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user

Re: Help: Housing Construction

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

OK. Seems like it's piling on more complexity.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Help: Housing Construction

Valued Contributor
Valued Contributor

This is not possible in the Sheet metal environment as this is not possible in realy life, you would be better off doing it in part then thinwall command maybe.

 

What are you making and out of what matrerial. 

 

Some kind of brass welded housing? or just a thermoplastic injection moulded cover?

Consultant - Design Majenta PLM - ST10/MP03