Cancel
Showing results for 
Search instead for 
Did you mean: 

Help Needed for converting DFT file to DXF

Experimenter
Experimenter

Hi Mates:

 

I am trying to convert a dft into dxf file but not able to do that if anyone here can help or convert the attached file that would be appreciated.

 

Thanks,

 

Looking forward for your help Guys.

11 REPLIES

Betreff: Help Needed for converting DFT file to DXF

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

 

 

You have tried to "Save As"  with changing the document typ to DXF/DWF?

 

 



regards
Wolfgang

Betreff: Help Needed for converting DFT file to DXF

Experimenter
Experimenter
i am having translator error while opening the file. So please if you help me do it.

Betreff: Help Needed for converting DFT file to DXF

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

 

 

 

maybe first going to the Options and run through all the option settings, save it into a new option INI file and then start the translation might help?

 



regards
Wolfgang

Betreff: Help Needed for converting DFT file to DXF

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,


OK,


just seen  that I 'm not able to open the draft file itself!

 

So question is, what version (although I did the test with ST9 which should open every SE file) are You using?

 

Or, do You have an academic version of SE?

 

Or ist the file itself corrupt?

 



regards
Wolfgang

Betreff: Help Needed for converting DFT file to DXF

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

 

just seen, that Your file only is 8kB in size which IMHO is much to small for a Solid Edge draft file, isn't it?

 



regards
Wolfgang

Betreff: Help Needed for converting DFT file to DXF

Experimenter
Experimenter
Still the same error.
If you convert the file i'll be highly obliged. My work is pending due to this since last week.

Betreff: Help Needed for converting DFT file to DXF

Experimenter
Experimenter

yes i have accademic verion of SE   (ST6)..................

giving error '' N0 TRANSLATOR IS AVALIBLE FOT THIS FILE TYPE  ''   help me 

Betreff: Help Needed for converting DFT file to DXF

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi,

I think this is not Solid Edge Draft document. I tried it open in academic ST9 version, with no success.

But when I looked in the file (simply opening it in notepad), there is a some sort of header with information:

pic1.png

It is look like some NC programm. Quick googling shows this is probably file from Metalix CAD/CAM solution called cncKad (link).

 

Ota

Betreff: Help Needed for converting DFT file to DXF

Experimenter
Experimenter
cncKad meatalix inc software is used