Cancel
Showing results for 
Search instead for 
Did you mean: 

Help creating model of twisted wire pair

Genius
Genius

I am struggling to create a model of a twisted wire pair.

 

Wire insulation is 2.16mm OD, conducter is 0.64 mm OD

 

Twist is 2 twists per 25.4mm

 

2 conductors to be as close together as possible.

 

I have tried a helix projection, but the rusult is not a round profile.

 

Any suggestions or guidance?

 

2 pictures attached, one of a 2d representation, another of end profile of helix result.

 

Using ST7 MP11

 

Gary Dinges | Mechanical Design Engineer II | Probes & New Product Development Emerson Climate Technologies | Therm-O-Disc, Inc.| 1320 South Main Street | Mansfield | OH | 44907 | USA T +1 419 525 8554 gary.dinges@emerson.com

7 REPLIES 7

Re: Help creating model of twisted wire pair

Gears Phenom Gears Phenom
Gears Phenom

I would use the twist option in the swept protrusion tool.

Have a look at the model in attachments.

 

double twisted wire.png

 

Francesco

Re: Help creating model of twisted wire pair

Genius
Genius

Thank You !!

 

That worked.

 

Gary

Re: Help creating model of twisted wire pair

Experimenter
Experimenter

Can you please exaplain how to create double twisted Wire pair in UG NX 11.  ?

Highlighted

Re: Help creating model of twisted wire pair

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Krishna_Prasad

 

 

 

 

Solid Edge or NX, this is here the question!

 

Post is in SE forum

 

regards
Wolfgang

Re: Help creating model of twisted wire pair

Experimenter
Experimenter

Hello Wolfgang,

We need to create using NX.

 

Thnaks & Regards,

Krishna Prasad

Re: Help creating model of twisted wire pair

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Krishna_Prasad

 

 

 

then I would suggest to better post that question in the NX forum rather than here.

We do a lot here in Solid Edge but I suppose we are limited in NX skills, at least most of us.

 

 

regards
Wolfgang

Re: Help creating model of twisted wire pair

Experimenter
Experimenter

Thank you