Cancel
Showing results for 
Search instead for 
Did you mean: 

Help with a loft

Valued Contributor
Valued Contributor

Hi,

 

I'm trying to connect these two cylinders with an elliptical rod.  I started with the smaller cylinder and sketched an ellipse on the right plane (yz).  I created a plane coincident with yz and placed it at the center of the larger cylinder and sketched a longer ellipse on it.  I used the Loft tool to make the connection.  Since the plane are at the centers of the cylinder, the loft extnded into the cylinder.  The larger cylinder was easy.  I clicked on the loft face and used the arrow to move it to the edge of the hole in the cylinder.  I couldn't do the same thing with the smaller cylinder.

 

I don't know much about Live Rules so I disabled them, but it still wouldn't work.

 

loft.png

 

 

6 REPLIES 6

Re: Help with a loft

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there,

 

Why not just add the end holes in afterwards?  [for where you're at now, I'd just delete the holes & replace them]

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Betreff: Help with a loft

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

 

and what's with selecting those 3 surfaces from the right and try to delete them?

 

Will this work?

 

 

regards

Wolfgang 

regards
Wolfgang

Re: Help with a loft

Valued Contributor
Valued Contributor

@SeanCresswell

 

I thought about that, but this is just an exercise and my goal is learn how to make changes in synchronous mode.  I just can't figure out why I can do it to one side, but not the other.

Betreff: Help with a loft

Valued Contributor
Valued Contributor

@hawcad

 

Are you talking about deleting the part that protrudes into the hole?  I don't think that's possible since it's part of the rod.

 

lfot2.png

Betreff: Help with a loft

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

 

 

no, I don't think so.

Since synchronous has no history, so there is no rod at thst moment.

 

More I think, that there are more surfaces than the one front plane.

And You must select all of them.

 

 

 

 

 

 

regards Wolfgang 

regards
Wolfgang
Highlighted

Betreff: Help with a loft

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

 

 

no, I don't think so.

Since synchronous has no history, so there is no rod at thst moment.

 

More I think, that there are more surfaces than the one front plane.

And You must select all of them.

 

 

 

 

regards Wolfgang 

regards
Wolfgang