Cancel
Showing results for 
Search instead for 
Did you mean: 

Help with moving origin & element properties

Not applicable
I started making a drawing, then decided it would be easier to move the origin, so as to set the origin on one corner on one of the elements.

I am able to do that, but the element properties still show the xy start/end points based on the old origin. How do I get them to update to the new origin? Or do I need to start over, but move the origin first?
1 REPLY

Re: Help with moving origin & element properties

Not applicable
The grid origin is only an origin for the grid lines and points.
It helps with snapping to the grid.
This grid origin has nothing to do with the object definitions such as
endpoints of lines.
Regards,
Rick B.