Cancel
Showing results for 
Search instead for 
Did you mean: 

Hide components keyboard shortcut

Builder
Builder

Is there a keyboard shortcut key that will hide components in an assembly ? I have always thought the 'Hide' and 'Show Only' should not be right next to each other in the RHMB menu as the 'Show Only' can often be accidentally clicked instead of 'Hide' and there is no undo this

10 REPLIES 10

Re: Hide components keyboard shortcut

Solution Partner Legend Solution Partner Legend
Solution Partner Legend
There is not a keyboard shortcut by default but you can create your own if you want. When you're in an assembly go into the customize menu and select the Keyboard tab. Change the Choose command from dropdown to All commands and then you can create your own shortcut for Hide.

Re: Hide components keyboard shortcut

Builder
Builder

Works a treat thanks Woman Happy

Re: Hide components keyboard shortcut

Pioneer
Pioneer

I want to add TAB key to hidening solid. I cannot find this option.

Do you have any clue?

Thanks.

I had done, I understood.

Re: Hide components keyboard shortcut

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Father

 

 

 

what is Your goal?

 

What and when should a tab key do something.

 

Shortcuts in SE need an additional special key like CTRL, SHIFT etc. together with the nominal key

 

 

 

regards
Wolfgang

Re: Hide components keyboard shortcut

Pioneer
Pioneer
I am using SolidWorks and SolidEdge, I so I want to have the same shortcut to hide solid.

Could you give me some clue how I can add any shortcut except TAB key to hide solid.

Thanks.
I had done, I understood.

Re: Hide components keyboard shortcut

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @Father

 

 

 

go to Customize and change the Keyboard code for Hide Design to whatever Your favorites may be.

See here as example the Alt+B command for HideDesign

So You also could use Alt+D for ShowDesign

 

20170614_1329.PNG

 

regards
Wolfgang

Re: Hide components keyboard shortcut

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi

 

 

 

 

...

 Keyboard ShortCuts are always a good way top automize Your workflow.

So for example I always have Alt+V to enter the Variable Table

 

Wether or not a Hide/Show BodyDesign will be usefull, this is to be desided by Yourself and by the individual user.

 

 

regards
Wolfgang

Re: Hide components keyboard shortcut

Phenom
Phenom

Why not just add the commands to the QAT ?

 

Assy QAT.JPG

HP Z420 16GB RAM
Quadro K4000
SE2019 MP5 on Windows 10 Pro 64.

Re: Hide components keyboard shortcut

Pioneer
Pioneer
Got it.

Thank you @hawcad.

I had done, I understood.