Cancel
Showing results for 
Search instead for 
Did you mean: 

Hide split lines in part on a draft

Creator
Creator

Hello, have altered a part using the split command, the part is shown on a draft drawing however the split line is visible, I want to hide this split line on the draft, how do I do this please ?

 

Using Solid Edge ST9

3 REPLIES 3

Re: Hide split lines in part on a draft

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @Anthony1,

 

Would the "Hide Edges" command work for you...?

 

ST9_Split [Draft_HideEdges].PNG

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Hide split lines in part on a draft

Creator
Creator

Hi Sean

 

Perfect, thank you Smiley Happy

Re: Hide split lines in part on a draft

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Very welcome @Anthony1.

 

Another way came to mind afterwards.

If you wanted to actually display one half of the split part, via the View Properties, Parts Display selection....see video. [could also set it as reference, and the selection would be unshaded, and have reference lines showing the where it should be.....I actually use this {video 2} display method quite a lot, albeit for my part drawings, for an Assembly]

 

(view in My Videos)

 

(view in My Videos)

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000