Cancel
Showing results for 
Search instead for 
Did you mean: 

Hiding "Error: No refernce" from Property Text Output

Creator
Creator

Hello Everyone.  We currently have a block on our drawing with some propety text that pulls information from the part's material properties.  It looks like this: %{Mtrl_Std/CM|R1}, %{Dim_Std/CM|R1}; %{Mtrl_Cond/CM|R1}

 

This works great for part and sheet metal files, but does not work for assembly files.  It shows "Error: No refernce" because those properties do not exist in the assembly file.

 

Material Block.png

Is there way to hide "Error: No refernce" without actually deleting the property text?

 

Thanks for your help.

 

 

11 REPLIES 11

Re: Hiding "Error: No refernce" from Property Text Output

Phenom
Phenom

We use a different template for sheet metal and assemblies, then that isn't a problem.

Re: Hiding "Error: No refernce" from Property Text Output

Gears Phenom Gears Phenom
Gears Phenom

prop.PNG

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"

Re: Hiding "Error: No refernce" from Property Text Output

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @nominus38

 

 

 

I personally prefer the "Show my error" using a simple "-" symbol to indicate that no property is available at the moment.

So this - for me - looks better than an "Error" but also shows me that it could be, that I have forgotten entering property info so far.

 

 

regards
Wolfgang

Re: Hiding "Error: No refernce" from Property Text Output

Creator
Creator

Thanks so much for the quick response.  Unfortunately, prop txt options are greyed out for me.  Any idea why it is not available?

 

Prop Txt Options.png

Re: Hiding "Error: No refernce" from Property Text Output

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @a2proven

 

 

 

to You use Insight?

 

 

I think I remember a situation where this options is not be available for an insight installation.

This could be changed somewhere in those settings

 

regards
Wolfgang
Highlighted

Re: Hiding "Error: No refernce" from Property Text Output

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @a2proven

 

 

 

if this is not the reason, then YOu can try it from the hard core side.

 

Change the registry settings for SOlid Edge - Current USer

 

 

You will find it under Global

 

20170811_1917.PNG

 

 

 

Change the "Display Property Text Error String" to 2

0 will be no errors

1 is system error and

2 is user error message

 

regards
Wolfgang

Re: Hiding "Error: No refernce" from Property Text Output

Creator
Creator

We do not use Insight, we use TeamCenter.  I am looking through the Admin XML file right now to see if there is a setting for this.  I would rather not do a reg edit.  Thanks for the response.

Re: Hiding "Error: No refernce" from Property Text Output

Creator
Creator

Well I found where this options is being blocked by our admin file.  Thanks again for your assistance in the is matter.

 

Pro Txt Admin.png

Re: Hiding "Error: No refernce" from Property Text Output

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @a2proven

 

 

welcome to be able helping!

 

 

So changing this value in the admin file will change it for the users too?

 

 

regards
Wolfgang