Cancel
Showing results for 
Search instead for 
Did you mean: 

Hole Command Question

Valued Contributor
Valued Contributor

Greetings,

 

 

Why doesn't the Solid Edge hole command have  ready to use standard tables for countersink, counterbore, and simple hole (loose fit, normal fit, tight fit etc) ?? 

 

Otherwise the hole command has an excellent workflow but why is this feature in the command missing?

 

Is this some kind of an oversight on my part? I understand the saved settings approach after you populate the fields with the desired values from the drop downs but there should be standard tables to choose from that populate these values so you don't have to "build" your hole specs and then save them in a mixed list.

 

Please enhance this command.

 

Regards,

 

Craig

2 REPLIES

Re: Hole Command Question

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
I understand what you are saying and you're not overlooking anything. Our machine designers where wanting the same. FYI, you need to call GTAC or your VAR to log an enhancement request. You can't do it here...


Ken
Production: SE 2019 MP4, Testing: SE 2020
http://Grundey.blogspot.com

Re: Hole Command Question

Valued Contributor
Valued Contributor
Ok. Thanks for the reply!