Cancel
Showing results for 
Search instead for 
Did you mean: 

Hole Count by Size?

Pioneer
Pioneer

Hey guys.

I'm trying to dimension the holes of my flat layout drawing in the draft environment.

I want it too look like, for example,  3-ø0.25

where it INCLUDES the quantity of that size hole (qty=3 in this example)

 

Thanks,

Jeff

1 REPLY

Re: Hole Count by Size?

Honored Contributor
Honored Contributor

Because of the work involved with that, I have gone to using the hole tables. The hole tables are one of the great and working features of the program other than you can't fully control row hight of the tables.