Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Hole Table not distinguishing between holes of different depth

Creator
Creator

Partial workaround (threaded holes only):

 

In the Hole Options dialogue, if you define one hole type using the Internal minor diameter and another using the nominal diameter they get there own table entry, there's also the tap drill diameter, so you can probably get three depths for the same thread size.

 

They end being displayed slightly differently to each other in the drawing, but I can live with that... just.

Re: Hole Table not distinguishing between holes of different depth

Creator
Creator

Finally a response from Siemens: 

 

"The customer request for filtering is very specific, so we are unlikely to include in the near future.

Hole table can be placed with some defined options only and currently there is no option to consider grouping based on multiple parameters like SIZE and DEPTH. "

 

So dont hold your breath... 

 

I really thought this would be quick and easy to implement. I suppose not enough users are asking for this. 

Re: Hole Table not distinguishing between holes of different depth

Valued Contributor
Valued Contributor

I have been holding my breath for this...

I'm as blue as a smurf!

-Russ