Cancel
Showing results for 
Search instead for 
Did you mean: 

Hole call out for a threaded and simple hole

Valued Contributor
Valued Contributor

I have a two holes that are 65 deep but have a 25 deep thread on it, what do i need to do to set the callout to show both the depth of the thread and hole? 

at the moment it only shows the thread depth. 

Capture.PNG

its the first and second from the left 

Capture 1.PNGCapture 3.PNG

Regards,

MagRiz
(ST9 User Est 01.18)
7 REPLIES 7

Re: Hole call out for a threaded and simple hole

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

%ZH or %HD will show the depth of the tap hole. %HS will show the tap drill diameter.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Hole call out for a threaded and simple hole

Gears Phenom Gears Phenom
Gears Phenom
Highlighted

Re: Hole call out for a threaded and simple hole

Valued Contributor
Valued Contributor

@bshand

 

hi ive done that but it adds the depth twice when the hole is fully threaded 

Capture.PNG

Regards,

MagRiz
(ST9 User Est 01.18)

Re: Hole call out for a threaded and simple hole

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Not seeing what your feature callout says I can only surmise that you have two depth callouts in your callout.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Hole call out for a threaded and simple hole

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Try this: The callout is below its symbology...ThdHoleDepth.JPG

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Hole call out for a threaded and simple hole

Valued Contributor
Valued Contributor

@bshand

Thanks that works, i added a return and added the word drill and thread to it too.

 

 

Regards,

MagRiz
(ST9 User Est 01.18)

Re: Hole call out for a threaded and simple hole

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@MagRiz, Good. Maybe a diameter symbol for the drill value too?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200