Cancel
Showing results for 
Search instead for 
Did you mean: 

Hole features on Different Layers

Experimenter
Experimenter

Hi,

 

Is it a possibiliy either with a work around or within the solid edge work flow to:

 

Create a part component with various hole depths in potentially different faces of the part and when brought into the draft enviroment for the varying hole depths to be allocated there own layer (10mm depth one layer  / 8mm another etc..), this would then be exported to dxf (I know i can alter the layers here but i am trying to avoid this as human error is ever present).

 

Any ideas appreciated, i am a bit stuck at the moment.

 

Thanks for any help

 

 

Mark

3 REPLIES 3
Highlighted

Re: Hole features on Different Layers

I bet you could put the depth callouts on different layers, but if you're bringing a 3D part into the draft environment I don't think you can split it like that.  I might be mistaken, but I'm under the impression that the part as shown in the draft environment is a cohesive whole and can't really be fiddled with like that.

Re: Hole features on Different Layers

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The only way this could be done is by automating it with a macro/add-in written in VB or C++



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Hole features on Different Layers

Experimenter
Experimenter
Thanks for the replies. I will look into the programming method.